"Static" and "Dynamic" EDS files.
---------------------------------

File labeled 'static' contains list of static connection pairs in the connection manager object.
File labeled 'dynamic' contains only one connection in connection manager object. This connection can be configured 
via parameters to connect to any input/output instance pair.

NOTE: EDS version in file name was changed from format "Vx.yy" to "YYYYMMDDD".

Vacon100_EIP_EDS_20180521
----------------------

Vacon100_EIP_EDS_20180521 shall be used with following or newer Vacon 100 firmware versions.

Vacon 100 INDUSTRIAL and Vacon 100 X: FW0072V021
Vacon 100 FLOW: FW0159V014

Vacon100_EIP_EDS_v1.05
----------------------

Vacon100_EIP_EDS_v1.05 shall be used with following or older Vacon 100 firmware versions:

Vacon 100 INDUSTRIAL and Vacon 100 X: FW0072V020
Vacon 100 FLOW: FW0159V013

How to see Vacon 100 firmware version?
--------------------------------------

Vacon 100 firmware version information can be checked from Vacon 100 panel or by using VaconLive PC-tool. Menu structure: Diagnostic -> Software Info -> Software package.