Date:   August 13, 2026

Updates:
-Support of up to 20 PCD’s (process data)
-New GSDML file in accordance with the PNO Schema 2.45. 
-GSDML file now handles the process data as sub module, where all previous versions were using modules.
-Modular configuration of telegrams, which helps in optimizing the process data usage. 

Info:
For MCA120 PROFINET firmware versions 1.xx and 2.xx please use the GSDML file located in the obsolete version folder 
The obsolete versions of the GSDML file, is not recommended to be used in new systems.
The obsolete version is included for support of old legacy controller systems and old firmware versions only.

GSDML-V2.45-Danfoss-FC-20260113
Compaible SW version: 7.21 and later