For each package there are 4 GSD files available, which support 4 different PROFINET GSD schema versions: 2.31, 2.35, 2.42 and 2.45.
The highest number is based on the latest released schema version and recommended to be used. If a given PROFINET I/O controller doesn't support this version, then one of the two legacy versions should be possible to use.
 
The latest released GSD files are backward compatible with previous versions.
 
Please note, that the information in the latest released GSD files are only supporting the corresponding released application software version. It will be possible to use these files with previous versions of the iC7-HVACR Drive, but the information in these files, can't be guaranteed to match the application software.
 
*************************************************************
 
Version history:
 
GSDML-Danfoss-iC7-HVACR-20260126: This file is released with the release of iC7-HVACR products iC7_HVACR-2026.3.3-GR.1

GSDML-Danfoss-iC7-HVACR-20260821: This file is released with the release of iC7-HVACR products iC7_HVACR-2026.9.23-26B.1